See Editing Device Information.
Field |
Description |
---|---|
Recipients |
List of recipients. |
Add |
Use to add a recipient. See Notification Recipient Screen. |
Remove |
Removes the recipient from the list. |
|
Moves the selected recipient up in the list of recipients. |
|
Moves the selected recipient down in the list of recipients. |
Details |
Opens the Notification Recipient dialog box, which displays details of the recipient. See Notification Recipient Screen. |
Save |
Saves changes to the information in the screen. |
Cancel |
Exits the screen without saving changes |
|
Opens the help system. |