See Setting up Device Notification.
Field |
Description |
---|---|
ID |
Indicates the ID of the device you want to send a notification to. ID field when selected. |
IP Address |
Indicates the IP address for the device you want to send notification to. Following fields when selected:
|
Broadcast |
Indicates if you want to broadcast the notification. Displays the following fields when selected:
|
MSTP Address |
Indicates if you want to send a notification to another controller. Following fields when selected:
|
Process ID |
Indicates the process ID of the device that receives the event notification messages. |
Day Selection |
Indicates the days you want the system to send notifications. |
Time Selection |
Indicates the time frame you want the system to send notifications. |
Notify on these Transitions |
Indicates the type of events to send notification: Off Normal, Fault, and Normal. |
Notification Messages Should Be |
Indicates if notifications need to be confirmed by a user. |