Event Log - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 16.0

Controller Tool Help

Product
Controls > Control Tools > Controller Configuration Tool
Document type
User Guide
Document number
LIT-12011147
Version
16.0
Revision date
2023-10-02

Use the Event Log - Details tab to set up the behavior of the Event Log - Events tab information. Use the Event Log - Events tab to view events. You can only view the Events tab when you are in Commissioning mode. See Viewing Event Logs.

Table 1. Event Log - Details Tab

Field

Description

Object

Name

Indicates the name of the event log.

Description

Indicates the description of the event log.

Enabled

Indicates if the event log is enabled (True) or disabled (False).

Object Identifier

Indicates the read-only BACnet object identifier for the event object.

BACnet

Buffer Size

Specifies the maximum number of records the event buffer can hold. This value is the total number of events that appear in the Event View during commissioning. The default value is 100 (maximum number of records).

You can only edit the buffer size in Configuration mode.

Reliability Indicates if the Event Log is reliable.
Status Flags Indicates Event Log status: In Alarm, Fault, Overridden, OutOfService.

Start Time

Specifies the time and date to enable logging when the Enabled attribute is set to True.

Stop Time

Specifies the time and date to disable logging.

Stop When Full

Specifies whether logging ceases when the buffer is full. When set to True, logging ceases and all accumulated samples remain in the buffer. When set to False, logging continues.

Total Record Count Indicates the total number of events in the log. You can view this value in the Details panel during Commissioning mode.
BACnet Intrinsic Alarming

Intrinsic Alarming Defined

Enables (True) or disables (False) BACnet intrinsic alarming for this object.

Acked Transitions Indicates if the Event Log has acknowledgment transitions pending.

Event Enable

Determines whether notifications are enabled for To Off Normal, To Fault, or To Normal events.

Event State Indicates the current state of the event log.
Last Notify Record

Indicates the sequence number associated with the most recently collected record whose collection triggered a notification.

Notification Class

Specifies the notification class used for handling and generating event notifications for this object.

Notify Threshold

Indicates when notification occurs based on the value of the Records Since Notification attribute.

Notify Type

Indicates if the notifications generated by the object are Events or Alarms.

Records Since Notify

Indicates if the notifications generated by the object are Events or Alarms. This attribute is required if the object supports intrinsic reporting.

Table 2. Event Log - Events Tab (Commissioning Mode Only)

Field

Description

Time

Indicates the time of the event occurrence.

Object

Indicates the object that event is associated with.

To State

Indicates the type of event state: Normal, Off Normal, High Limit, or Fault.

Priority

Indicates the importance of the event message and determines when the event message appears. Event messages with a lower priority number are of a higher importance or are more critical than event messages with a higher priority number.

Event Time

Indicates the time of occurrence of the last event transition.

Value

Indicates the value of the event or alarm. For example, On or Off, or 80 degrees.

Unit

Indicates the unit of measurement for the event or alarm value.

Message

Indicates the body of the alarm or event message.