Configuring Advanced Controller Features - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 16.0
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
Advanced features for field equipment controllers include schedules, calendars, alarms, and trends. In Configuration or Commissioning mode, you can use the Advanced tab to configure these features. When you configure advanced features, you can do the following:

The Calendars, Schedules, Trends, and Alarms and Notification features can be used during a stand-alone commissioning session of the advanced field controller, or these features can be integrated into supervisory system as BACnet® objects.

If these features are integrated into a supervisory system, you can edit feature attributes in both a local commissioning session or from the supervisory system user interface.