Issuing a Flow Override Command - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 16.0

Controller Tool Help

Product name
Controller Configuration Tool
Document type
User Guide
Document number
LIT-12011147
Version
16.0
Revision date
2023-10-02

Procedure

  1. In the details view of the Balancer Override SD module, click Flow Override. The Flow Override Command dialog box appears.
  2. Select a value from the menu. For example, select Supply Duct Max to drive the VAV Box Controller to the maximum cfm.
  3. Click Send to issue the command.

    Return to the Using the Balancing Feature section.