Editing the Balancing Attributes - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 16.0

Controller Tool Help

Product
Controls > Control Tools > Controller Configuration Tool
Document type
User Guide
Document number
LIT-12011147
Version
16.0
Revision date
2023-10-02

Procedure

  1. Right-click the Balancer Override SD module and click View Details.
  2. Click Edit.
  3. Modify the attributes as desired (for example, change the flow setpoints).
    Note: Click Cancel to exit Edit mode without applying changes.
  4. Click Apply. The changes are made and the system exits Edit mode.

    Return to the Using the Balancing Feature section.