Calculating the K-Factors - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 16.0

Controller Tool Help

Product name
Controller Configuration Tool
Document type
User Guide
Document number
LIT-12011147
Version
16.0
Revision date
2023-10-02

Procedure

  1. In the details view of the Balancer Override SD module, click Calculate K-Factors. The Calculate K-Factors Command dialog box appears.
  2. Select the duct from the Duct Selection menu.
  3. Enter the proper value in the Measured Flow field.
  4. Click Send. The values on the Balancer tab update according to this new value.

    Return to the Using the Balancing Feature section.