Making a MAP 4.2+/BACnet Router Connection - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 16.0
Controller Tool Help
- Product name
- Controller Configuration Tool
- Document type
- User Guide
- Document number
- LIT-12011147
- Version
- 16.0
- Revision date
- 2023-10-02
Procedure
-
Open the tool.
-
Click Commission. The Commission Device Wizard appears.
-
Select application and connection attributes, then click Next.
-
Select the device and click Next. The Commission Device Summary dialog box appears.
Notes:
- If you have selected Current Application, only the Field Device defined in your CAF appears in the selection list.
- Do not use 1001 for the MS/TP Network Number. The MS/TP Network Number 1001 is reserved for Johnson Controls IP network connections.