Making a Direct Ethernet Connection - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 16.0
Controller Tool Help
- Product
- Controls > Control Tools > Controller Configuration Tool
- Document type
- User Guide
- Document number
- LIT-12011147
- Version
- 16.0
- Revision date
- 2023-10-02
- Open the tool.
- Click Commission. The Commission Device Wizard appears.
- Make your application and connection attribute selections and click Next.
- Select the device and click Next. The Commission Device Summary dialog box appears.
Notes:
- Verify you are on the same subnet as your IP controllers to use a Direct Ethernet connection.
- If you have selected Current Application, only the Field Device defined in your CAF appears in the selection list.