Adjust Refresh Rate Dialog Box - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 16.0
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
Table 1. Adjust Refresh Rate Dialog Box

Field

Description

Simulation Refresh Rate Slider Bar

Adjust the simulation refresh rate to any length of time from 1 second to 60 seconds.

Commissioning Refresh Rate Slider Bar

Adjust the commissioning refresh rate to any length of time from 1 second to 60 seconds.

Highlight Duration Slider Bar

Adjust the highlight duration rate for changing parameter values displayed in the Commissioning and Simulation modes. Highlight duration refresh rates range from 1 to 10 in length.

Note: The highlighting change feature can be turned on or off from the Commissioning mode's or Simulation mode's control bars.

OK

Saves and closes the dialog box.

Cancel

Closes the dialog box without applying the changes.

Opens the Help system.