System and Device Connections - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 16.0

Controller Tool Help

Product
Controls > Control Tools > Controller Configuration Tool
Document type
User Guide
Document number
LIT-12011147
Version
16.0
Revision date
2023-10-02

Five connection options are available: Supervisor Passthru, Bluetooth, MAP 4.2+/BACnet Router, ZigBee, and Direct Ethernet. See Connections in the Transfer Operations section for details on these options.