Control Bar - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 16.0

Controller Tool Help

Product name
Controller Configuration Tool
Document type
User Guide
Document number
LIT-12011147
Version
16.0
Revision date
2023-10-02
Commissioning mode offers a control bar for easy control and detailed viewing. The Commissioning Control Bar displays one of two Commissioning Time Sources based on the user's preference of the Device Time or Your Computer Time. In addition to displaying source times, you can start Test Mode by selecting the Start Test Mode check box to enable and disable the Highlight Changes feature.
Figure 1. Commission Mode—Control Bar

Users can toggle between a full-length horizontal control bar at the bottom of their window or a collapsed version of the control bar by clicking the Minimize () icon or the Maximize () icon.