Balancing Feature - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 16.0
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
The details view of the Balancer Override module includes an attributes table and task buttons to autocalibrate VAV Box Controllers and set flow constants. This feature appears in Commissioning mode only for VAV Box Controllers. The task buttons of the Balancer Override module details view are active only when in the Test mode; however, you do not need to be in Test mode to edit the attributes table.

The Balancer Override module is described in the Balancer Override topic of the State Generation Modules section . See the Using the Balancing Feature section for information on balancing tasks.