Plant Layout Configuration (SP) - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 16.0

Controller Tool Help

Product
Controls > Control Tools > Controller Configuration Tool
Document type
User Guide
Document number
LIT-12011147
Version
16.0
Revision date
2023-10-02
The selection options for Plant Layout Configuration are:

  • Cooling Only Plant: This option configures a Simple Central Plant with cooling only.

  • Heating Only Plant: This option configures a Simple Central Plant with heating only.

  • Four Pipe Plant (Heating and Cooling): This option configures a Simple Central Plant with heating and cooling. It provides for seasonally controlled changeover or simultaneous heating and cooling.

  • Two Pipe Plant (Heating and Cooling): This option configures a Simple Central Plant with heating and cooling.

    • Water Source Heat Pump Loop: This option configures a special plant to provide a central loop for water source heat pumps.

  • Cooling Configuration: This section allows you to configure the cooling portion of the Simple Central Plant.

    • One Chiller: This option determines if you have a mechanical device that provides chilled water.

    • Primary Chill Water Pumps: This option defines the number of chilled water pumps in the system.

      • One Pump

      • Two Pumps

      • Variable Speed

    • Condenser Water Pumps

      • None (Air Cooled Chiller): This option is for chillers using air-cooled condensers. The chiller control panel is responsible for controlling the condenser fans.

      • One Pump

      • Two Pumps

    • Condenser Water System: The selection options for Condenser Water System are:

      • Tower Bypass Valve: This option allows a bypass valve to control condenser water temperature.

      • Cooling Tower Fan: This option allows a cooling tower to control condenser water temperature.

        • Single Speed

        • Two Speed

        • Three Speed

        • Variable Speed

  • Heating Configuration: This option determines if you have a mechanical device that provides hot water.

    • Hot Water Boiler: This option defines the number of 2-pipe pumps in the system.

    • Primary Hot Water Pumps: This option defines the number of hot water pumps in the system.
      • One Pump

      • Two Pumps

      • Variable Speed: If the pump(s) need speed control to maintain pressure in the piping loop, select this option.

    • Steam Boiler: This option determines if you have a mechanical device that provides steam.
    • Steam Heat Exchanger: This option determines if you have a heat exchanger that converts steam to hot water.
      • Two Inlet Valves: This option provides control for 2 inlet valves controlled in sequence to provide finer control for low load conditions.

      • Primary Hot Water Pumps: This section describes the pumps for the heat exchanger.
        • One Pump

        • Two Pumps

        • Variable Speed: If the pump(s) need speed control to maintain pressure in the piping loop, select this option.

  • 2 Pipe Configuration: This section defines the options for a 2-pipe Simple Central Plant

    • Primary Water Pumps: This option defines the number of 2-pipe pumps in the system.

      • One Pump

      • Two Pumps

      • Variable Speed: If the pump(s) need speed control to maintain pressure in the piping loop, select this option.