Heating Configuration (SP) - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 16.0
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
This section allows you to configure the heating portion of the Simple Central Plant

  • Hot Water Boiler: This option determines if you have a mechanical device that produces hot water.

  • Primary Hot Water Pumps: This option defines the number of hot water pumps in the system.

    • One Pump

    • Two Pumps

    • Variable Speed: If the pump(s) need speed control to maintain pressure in the piping loop, select this option.

  • Steam Boiler: This option determines if you have a mechanical device that provides steam.

  • Steam Heat Exchanger: This option determines if you have a heat exchanger that converts steam to hot water.

    • Two Inlet Valves: This option provides control for two inlet valves controlled in sequence to provide finer control for low load conditions.

    • Primary Hot Water Pumps: This section describes the pumps for the heat exchanger.

      • One Pump

      • Two Pumps

      • Variable Speed: If the pump(s) need speed control to maintain pressure in the piping loop, select this option.