Modules (SP) - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 16.0

Controller Tool Help

Product
Controls > Control Tools > Controller Configuration Tool
Document type
User Guide
Document number
LIT-12011147
Version
16.0
Revision date
2023-10-02

All Simple Plant applications use the core logic listed as follows:

Network Inputs
  • TUNING-RESET: This module is used to reset the tuning parameters to the default values present after the initial application transfer to the device.
Setpoint/Miscellaneous
  • PID Tuning Reset This module forces every output controller to reset the Proportional Band and Integral time of every PID to default values based on current process ID.