The selection options for Basin Options are:
-
Basin Level Alarm: This option monitors basin low level alarms.
-
Basin Heater Enable: This option generates BOs to command the basin heaters through the BAS.
-
Basin Water Temperature: This option monitors basin water temperatures.
-
Switch: This option monitors BI inputs for low temperature switches.
-
Analog Temperature: This option monitors AI inputs for temperature.
-
-
Basin Level Switch: This option monitors the basin levels.
-
Basin Makeup Valve: This option generates BOs to command basin makeup valves through the BAS.
If the No CW Piping (Air Cooled) node is selected, Basin Options cannot be selected.