Simple Central Plant Applications - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 16.0

Controller Tool Help

Brand
Johnson Controls
Metasys
Product name
Controller Configuration Tool
Document type
User Guide
Document number
LIT-12011147
Version
16.0
Revision date
2023-10-02
Language
English

A Simple Plant allows a configuration of a cooling only, heating only, or both cooling and heating plants. The Simple Central Plant (SP) application provides mechanical and control logic selections that match standard Simple Plant configurations.

Simple Plant applications allows applications to control a single chiller and boiler with associated pumps configured in a 4-pipe or 2-pipe distribution. Simple Plant applications support simple cooling, heating, or heating and cooling plants, including water source heat pump plants.