Heating System Enable (CH) - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 16.0

Controller Tool Help

Product
Controls > Control Tools > Controller Configuration Tool
Document type
User Guide
Document number
LIT-12011147
Version
16.0
Revision date
2023-10-02

The selection option for Heating System Enable is:

  • OA Heating Lockout: This option allows the system to be automatically enabled and disabled based on the outdoor air temperature.

  • Emergency Shutdown: This option allows the system to automatically shut down upon activation of a binary input.

  • Low Pressure Shutdown: This option allows the system to automatically shut down should the system pressure drop below a specified pressure.