Heat Exchanger Options (CH) - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 16.0

Controller Tool Help

Product name
Controller Configuration Tool
Document type
User Guide
Document number
LIT-12011147
Version
16.0
Revision date
2023-10-02

This section is for general options associated with heat exchanger systems.

The selection options for Heat Exchanger Options are:

  • Loop Bypass Temperature Sensor: This option monitors the loop bypass temperature.

  • Hot Water Supply Temp Per Heat Exchanger: This option monitors the leaving (supply) water temperature for each heat exchanger.

  • Hot Water Return Temp Per Heat Exchanger: This option monitors the entering (return) water temperature for each heat exchanger.

  • Steam Pressure Sensor: This option monitors steam pressure.

If Heat Exchangers is not selected, none of these options can be selected.