Zone Loop Options (CC) - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 16.0
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
The options for Zone Loop are:

  • Supply Temperature per Zone: This option adds a temperature sensor to monitor the Zone Loop supply temperature.

  • Return Temperature per Zone: This option adds a temperature sensor to monitor the Zone Loop return temperature.

  • Flow Switch per Zone: This option adds a binary input to monitor the flow in the Zone Loop.

  • Flow Sensor per Zone: This option adds an analog input to monitor the flow in the Zone Loop.