Condenser Options (CC) - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 16.0

Controller Tool Help

Product
Controls > Control Tools > Controller Configuration Tool
Document type
User Guide
Document number
LIT-12011147
Version
16.0
Revision date
2023-10-02

The selection options for Condenser Options are:

  • Common Return Temperature: This option monitors the condenser return water temperature.

  • Condenser Flow Sensor: This option monitors the condenser flow sensor.

  • Vibration Alarm per Tower: This option monitors the vibration alarm on each cooling tower.