Parallel Primary CW Pumps (CPO) - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 16.0

Controller Tool Help

Product
Controls > Control Tools > Controller Configuration Tool
Document type
User Guide
Document number
LIT-12011147
Version
16.0
Revision date
2023-10-02

In the following figure, the condenser water pumps are connected in a headered or parallel configuration so that any pump may be used with any chiller. The isolation valves are piped to the chillers in a dedicated configuration to prevent water from flowing through an inactive chiller.

Figure 1. Water-Cooled Condenser Headered System