Dedicated Primary CW Pumps (CPO) - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 16.0
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
In the following figure, the condenser water pumps are connected in a dedicated configuration. Each condenser water pump is connected to a specific chiller. The condenser water pumps are interlocked to its chiller such that the pump is started before the chiller is enabled.

Figure 1. Water-Cooled Condenser Dedicated System