Unit Reset Switch (CPO) - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 16.0

Controller Tool Help

Product
Controls > Control Tools > Controller Configuration Tool
Document type
User Guide
Document number
LIT-12011147
Version
16.0
Revision date
2023-10-02

The application has a unit reset input if any alarms or interlocks require a manual reset. At selection time, the user has the option to select either a hardware or network input for unit reset.