The selection options for Basin Options are:
-
Dedicated - one per tower: This option provides control if all the towers have individual basins.
-
Common Sump: This option provides control if all the towers share a common basin.
-
Basin Level Alarm(s): This option monitors basin low level alarms.
-
Basin Heater Enable(s): This option generates BOs to command the basin heaters through the BAS.
-
Basin Water Temperature(s): This option monitors basin water temperatures.
-
Switch(es): This option monitors BI inputs for low temperature switches.
-
Analog Temperature(s): This option monitors AI inputs for temperature.
-
-
Basin Level Switch(es): This option monitors the basin levels.
-
Basin Makeup Valve(s): This option generates BOs to command basin makeup valves through the BAS.
If the No CW Piping (Air Cooled) node is selected, Basin Options cannot be selected.