Box Flow Test Overview - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 16.0

Controller Tool Help

Brand
Johnson Controls
Metasys
Product name
Controller Configuration Tool
Document type
User Guide
Document number
LIT-12011147
Version
16.0
Revision date
2023-10-02
Language
English

Use the Box Flow Test to verify and diagnose the operation of Single Duct, Dual Duct, and Supply Exhaust applications. The Box Flow Test module provides the timing, output control, and data-gathering functions for testing the flow control performance of a VAV Box Controller application.

See Box Flow Test in the State Generators section for information on the Box Flow Test module.