Binary Value Commands - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 16.0
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
Table 1 describes the Binary Value object commands. For information about command priorities, see Command Priority Levels.

Table 1. Binary Value Commands

Name

Description

Operator Override

Replaces Present Value (Appears as O1) at the Operator Override priority with the value you enter in the command. The override has no effect if a higher priority value is in the Present Value attribute.
Note: This command is available only if the Binary Value is prioritized.

Operator Override Release

Releases an Operator Override command.
Note: This command is available only if the Binary Value is prioritized.

Release

Releases a specific priority of Present Value (Appears as O1).
Note: This command is available only if the Binary Value is prioritized.

Release All

Releases Priorities 3 - 15.
Note: This command is available only if the Binary Value is prioritized.

State 0

Releases command Priorities 9 - 15 and then writes State 1 to Present Value (Appears as O1) at Priority 16.
Note: This command is available only if the Binary Value is prioritized.

State 1

Releases command Priorities 9 - 15 and then writes State 1 to Present Value (Appears as O1) at Priority 16.
Note: This command is available only if the Binary Value is prioritized.