Binary Value Object - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 16.0

Controller Tool Help

Brand
Johnson Controls
Metasys
Product name
Controller Configuration Tool
Document type
User Guide
Document number
LIT-12011147
Version
16.0
Revision date
2023-10-02
Language
English

This object allows you to hold a binary value for other objects to reference. In the tool, a BV may be created as part of an SAB device to provide binary data points from that device (for example, Temporary Occupancy of the Network Sensor). Alternately, a Binary Value may be created as a reference point for a wireless sensor to write its value (typically to the mapped BV in the supervisory device).

For more information on the Binary Value object, see Binary Value Attributes and Binary Value Commands.