Binary Input Commands - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 16.0

Controller Tool Help

Brand
Johnson Controls
Metasys
Product name
Controller Configuration Tool
Document type
User Guide
Document number
LIT-12011147
Version
16.0
Revision date
2023-10-02
Language
English

Table 1 describes the Binary Input object commands.

Table 1. Binary Input Commands

Name

Description

In Service

Cancels the effects of an Out of Service command. This command changes Out of Service to False and reconnects the input to the hardware. Present Value (Appears as O1), Reliability, and Status values return to the last known value as reported before the Out of Service command.

Out of Service

Overrides Present Value (Appears as O1) for simulation or other purposes. This command changes Out of Service to True, Present Value to the value you specify, Status to Out of Service, and Reliability to Reliable. Present Value and Reliability are not connected to the hardware when the input is out of service, so this is the only time they are writable.