Analog Input Commands - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 16.0

Controller Tool Help

Product
Controls > Control Tools > Controller Configuration Tool
Document type
User Guide
Document number
LIT-12011147
Version
16.0
Revision date
2023-10-02

Table 1 describes the Analog Input object commands.

Table 1. Analog Input Commands

Name

Description

In Service

Cancels the effects of an Out of Service command. This command changes Out of Service to False and reconnects the input to the hardware. Present Value (appears as O1), Reliability, and Status values update at time specified in Update Interval.

Out of Service

Overrides Present Value (appears as O1) for simulation or other purposes. This command changes Out of Service to True, Present Value to the value you specify, Status to Out of Service, and Reliability to Reliable. Present Value and Reliability are not connected to the hardware when the input is out of service, so this is the only time they are writable.