Temperature Control Strategy (SZAHU) - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 16.0
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
Use this section to define the properties of any chilled water or hot water coils. The types of supported coils are proportional or incremental. Entering and Leaving Water Temperature sensors are also supported and add analog inputs for the sensors.