Separate Outputs (SZAHU) - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 16.0

Controller Tool Help

Product
Controls > Control Tools > Controller Configuration Tool
Document type
User Guide
Document number
LIT-12011147
Version
16.0
Revision date
2023-10-02

This option adds two AOs (OAD-O and RAD-O) to provide damper control for the unit mixing dampers. Control dampers in a complimentary fashion and use them as part of the discharge air temperature control strategy along with any heating or cooling coil.