Common Output (SZAHU) - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 16.0

Controller Tool Help

Product
Controls > Control Tools > Controller Configuration Tool
Document type
User Guide
Document number
LIT-12011147
Version
16.0
Revision date
2023-10-02

This option adds a single AO (MAD-O) to provide damper control for mechanically linked dampers or several actuators operating using the same signal. Use the dampers as part of the discharge air temperature control strategy along with any heating or cooling coil.