Configuration Options (MADD-MZ) - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 16.0

Controller Tool Help

Product name
Controller Configuration Tool
Document type
User Guide
Document number
LIT-12011147
Version
16.0
Revision date
2023-10-02

These selections allow the user to select the portion(s) of the Multizone logic to include in this system. The selection options are:

  • AHU Only

    • Zone Heating Valve Mode Output

    • Zone Staged Heating Mode Output

  • Zones Only

  • AHU + Zones