Optional Equipment (MADD-MZ) - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 16.0

Controller Tool Help

Product
Controls > Control Tools > Controller Configuration Tool
Document type
User Guide
Document number
LIT-12011147
Version
16.0
Revision date
2023-10-02

These selections provide monitor-only sensors for an optional pre-filter, final filter, or both.

The selection options for Optional Equipment are:

  • Pre-Filter

    • Filter Switch

    • Filter Differential Pressure Sensor

  • Final Filter

    • Filter Switch

    • Filter Differential Pressure Sensor

  • Return Filter

    • Filter Switch

    • Filter Differential Pressure Sensor

These options are not applicable if the Zones Only configuration type is selected.