Selecting this option shifts the heating and cooling setpoints to compensate for extreme outdoor air temperatures. This works similar to zone control reset by outdoor air temperature, with a large deadband so the setpoints are not modified while the outdoor air is between 50 and 75 °F.