Cycle During Occupied (MASD) - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 16.0
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
This feature causes the fan to cycle off during the occupied mode if there is no call for heating or cooling. This node is located here because only zone or return temperature control schemes allow this option. Discharge air control schemes require airflow to determine the need for heating or cooling.

If Discharge Air Temperature Reset by Zone or Return is selected, Cycle During Occupied cannot be selected.