Fan Status (MOA) (MASD) - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 16.0

Controller Tool Help

Product
Controls > Control Tools > Controller Configuration Tool
Document type
User Guide
Document number
LIT-12011147
Version
16.0
Revision date
2023-10-02

Selecting the option for Fan Status adds a binary input for the minimum outdoor air fan. You may select to restart the minimum outdoor air fan automatically or manually after the loss alarm is cleared. Selecting Manual Restart adds either a BI or Network Input to the system. This input must be commanded to restart the system.