Air to Air Heat Exchanger (MASD) - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 16.0

Controller Tool Help

Product
Controls > Control Tools > Controller Configuration Tool
Document type
User Guide
Document number
LIT-12011147
Version
16.0
Revision date
2023-10-02

The Air to Air Heat Exchanger is a mechanical heat exchanger that uses counter airflow to moderate incoming air temperature. When you select Modulated Bypass Dampers, this option adds bypass dampers to prevent freezing exhaust air.