Exhaust Fan Status (MASD) - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 16.0

Controller Tool Help

Product
Controls > Control Tools > Controller Configuration Tool
Document type
User Guide
Document number
LIT-12011147
Version
16.0
Revision date
2023-10-02

Selecting the option for Fan Status adds a binary input for the toilet exhaust fan. You may select to restart the exhaust fan automatically or manually after the loss alarm is cleared. Selecting Manual Restart adds either a BI or Network Input to the system. This input must be commanded to restart the system.