Shutdown AHU When Pump is in Alarm (MASD) - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 16.0

Controller Tool Help

Product
Controls > Control Tools > Controller Configuration Tool
Document type
User Guide
Document number
LIT-12011147
Version
16.0
Revision date
2023-10-02

For applications with Preheat pumps, the Shutdown AHU when pump is in Alarm option prevents the unit from starting if there is a fault in the preheat pump during cold weather.