Leaving Water Temperature (MASD) - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 16.0

Controller Tool Help

Product name
Controller Configuration Tool
Document type
User Guide
Document number
LIT-12011147
Version
16.0
Revision date
2023-10-02

Leaving Water Temperature can be selected when you need to monitor the coil return water or condensate temperature. This option adds an analog input for this sensor.