Hot Water or Steam (MASD) - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 16.0

Controller Tool Help

Product
Controls > Control Tools > Controller Configuration Tool
Document type
User Guide
Document number
LIT-12011147
Version
16.0
Revision date
2023-10-02

The section is used to define the properties of a hydronic coil. This section may be used for other types of heating coils, but some changes may be required. This section is designed to support water and steam coils.