Two Position Actuator (MASD) - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 16.0

Controller Tool Help

Product name
Controller Configuration Tool
Document type
User Guide
Document number
LIT-12011147
Version
16.0
Revision date
2023-10-02

Two Position Actuator can be selected if the coil is controlled by a two position valve that uses a binary output to open and close the valve. Two position preheat coil valves are only available with a Face and Bypass Damper to allow some air to bypass the coil in certain conditions. The face and bypass damper can be controlled using a Proportional Actuator or an Incremental Actuator.