The next two sections define the type of cooling coil in the air handler. Staged cooling may be used for staged DX cooling coils. Staged DX coils always include the no flow lockout logic.
Check Device Rotation to rotate the first stage so that the stages get approximately equal runtime.
Check First Stage Modulated to select up to four stages of cooling.
You can select up to 8 stages of cooling if the first stage is not modulated.