These selections provide the option for loading extra, monitor-only sensors.
The selection options for Optional Sensors are:
-
Position Feedback: This option provides feedback inputs for monitoring only purposes. If you want to generate an alarm or other functionality using the position feedback inputs, you must create custom coding to do so.
-
Modulated Damper Outputs
-
No Position Feedback
-
Analog Input per Output
-
Binary Input per Output
-
-
Modulated Valve Outputs
-
No Position Feedback
-
Analog Input per Output
-
Binary Input per Output
-
-
Two Position Damper Outputs
-
No Position Feedback
-
Binary Input per Output
-
Two Binary Inputs per Output
-
-
Two Position Valve Outputs
-
No Position Feedback
-
Binary Input per Output
-
Two Binary Inputs per Output
-
- VSD Outputs
- No Feedback
- Motor Speed (RPM)
- Drive Frequency (Hz)
- Motor Percent (%)
-
-
Outdoor Air
-
Temperature
-
Humidity
-
CO2 Sensor
-
Air Flow
-
Velocity Pressure (Pitot Tube)
-
Flow Measurement (Scaled)
-
-
-
Minimum Outdoor Air
-
Air Flow
-
Velocity Pressure (Pitot Tube)
-
Flow Measurement (Scaled)
-
-
-
Preheat Air Temperature
-
Mixed Air
-
Temperature
-
Humidity
-
CO2 Sensor
-
-
Cooling Coil Leaving Air Temperature
-
Reheat Coil Leaving Air Temperature
-
Discharge Air
-
Temperature
-
Humidity
-
CO2 Sensor
-
Static Pressure
-
Air Flow
-
Velocity Pressure (Pitot Tube)
-
Flow Measurement (Scaled)
-
-
Minimum Flow Protection For Staged Heating
-
-
Return Air
-
Temperature
-
Humidity
-
CO2 Sensor
-
Static Pressure
-
Air Flow
-
Velocity Pressure (Pitot Tube)
-
Flow Measurement (Scaled)
-
-
-
Relief Air
-
Air Flow
-
Velocity Pressure (Pitot Tube)
-
Flow Measurement (Scaled)
-
-
-
Zone
-
Temperature
-
Humidity
-
CO2 Sensor
-
-
Misc
-
Building Static Pressure
-
Heat Recovery Air Temperature
- Mechanical Room Temperature: This option adds an analog input for a zone sensor that monitors the temperature in the mechanical room.
-
If a Sensor is required for one of the selections made in the Mechanical System Selection, the option is not available here.
The Minimum Flow Protection for Staged Heating can be selected if Staged Preheat (in Mixed Air) or Staged Reheat is selected and the Discharge Flow is available (either due to selecting Return Fan Volume Matching or an optional Discharge Flow sensor).