These selections provide the logic to control a Cooling coil.
The selection options for Coils (Cooling - Cold Deck) are:
Cooling - Cold Deck
- Shutdown on Alarm: This option places the system in shutdown mode when the condensate alarm is active.
Cooling Lockout from Outdoor Air
DX Cooling
-
Device Rotation
- First Stage Modulated: When you check this, you can select up to four stages of cooling.
-
Number of Stages
-
One Stage
-
Two Stages
-
Three Stages
-
Four Stages
-
Five Stages
-
Six Stages
-
Seven Stages
-
Eight Stages
-
Chilled Water
-
Proportional Actuator
-
Incremental Actuator
-
Two Position Actuator
-
Face and Bypass Damper
-
Proportional Actuator
-
Incremental Actuator
-
-
-
Entering Water Temperature
-
Leaving Water Temperature
-
Coil Pump
-
Pressure/Flow Boost
-
Low Temperature Circulation
-
Pump Status
-
Loss of Status Strategy
-
Automatic Restart
-
Manual Restart
-
Unit Reset Switch (BI)
-
-
-
-
Alarm Management
-
Lockout Switch
-
Motor Overload Tripped
-
Automatic Restart
-
Manual Restart
-
Unit Reset Switch (BI)
-
-
-
-
Blocking Protection: This option provides monitoring of the command to a motor (typically a pump). If the command is off for an extended period of time (for example, 7 days), the motor starts for a short time (for example, 30 seconds). This feature prevents blocking (that is, it prevents the motor from seizing up).
-
-
Shutdown Strategy
-
Off
-
Protect Coil Based on Outdoor Air Temperature
-
User Defined Position
-
-
Loss of Airflow Strategy
-
Off
-
Remain in Control
-
Protect Coil Based on Outdoor Air Temperature
-
User Defined Position
-
-
Unreliable Sensor Operation
-
Off
-
Hold
-
Protect Coil Based on Outdoor Air Temperature
-
User Defined Position
-
The Loss of Airflow Strategy options are available only when the Automatic Restart option for the Supply Fan Status Loss of Airflow Strategy is selected.