These selections provide the logic to control a Heat Recovery Enthalpy Wheel or Glycol Loop.
The selection options for Heat Recovery are:
Enable Type
-
Dry Bulb
-
Enthalpy
- Always On
Enthalpy Wheel
-
Single Speed
-
Modulated Bypass Dampers
-
-
Variable Speed
-
Bypass Damper BO
-
-
Wheel Status
-
Loss of Status Strategy
-
Automatic Restart
-
Manual Restart
-
Unit Reset Switch (BI)
-
-
-
-
Alarm Management
-
Lockout Switch
-
Frequency Converter Fault
-
Automatic Restart
-
Manual Restart
-
Unit Reset Switch (BI)
-
-
-
Motor Overload Tripped
-
Automatic Restart
-
Manual Restart
-
Unit Reset Switch (BI)
-
-
-
Belt Alarm
-
Automatic Restart
-
Manual Restart
-
Unit Reset Switch (BI)
-
-
-
-
Blocking Protection/Cleaning Mode: This option provides cleaning mode functionality. If the wheel is off for an extended period, the wheel turns on for a short time to keep the wheel free of dirt and dust.
Glycol Loop
-
3-Way Valve
-
Proportional Actuator
-
Incremental Actuator
-
-
Circulation Pump
-
Pump Status
-
Loss of Status Strategy
-
Automatic Restart
-
Manual Restart
-
Unit Reset Switch (BI)
-
-
-
-
Alarm Management
-
Lockout Switch
-
Motor Overload Tripped
-
Automatic Restart
-
Manual Restart
-
Unit Reset Switch (BI)
-
-
-
-
Blocking Protection: This option provides monitoring of the command to a motor (typically a pump). If the command is off for an extended period of time (for example, 7 days), the motor starts for a short time (for example, 30 seconds). This feature prevents blocking (that is, it prevents the motor from seizing up).
-
Air to Air Heat Exchanger
-
Modulated Bypass Dampers