Temperature Control Strategy (OADD) - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 16.0

Controller Tool Help

Product
Controls > Control Tools > Controller Configuration Tool
Document type
User Guide
Document number
LIT-12011147
Version
16.0
Revision date
2023-10-02

These selections provide the logic for determining the setpoints of the Cold Deck and Hot Deck temperature control loops. The Hot Deck Setpoint options apply only if a Hot Deck heating coil is selected.

The selection options for Temperature Control Strategy are:

  • Fixed Hot, Cold, or both Deck Temperatures

  • Hot, Cold, or both Deck Temperature Reset from OA-T

  • Hot Deck Temperature Reset from EA-T